To find the full load current for your single phase motor running at normal speed and torque, use your motor's horsepower and rated motor voltage to find the full load current in amps in the chart below.
The voltages listed are rated motor voltages. The listed currents are for system voltage ranges of 110 ‑ 120 and 220 ‑ 240.
TABLE 430.248, 2020 NEC®
Warning: For safety, call a licensed electrician and consult the NEC®. All licensed electricians have passed examinations covering the National Electric Code®, know state and local building codes, and may carry insurance to cover damages.