The Electric Times - Current Sales Events at Elliott Electric Supply



 
Electric Times banner header
Electric Times banner


December 2025 Electric Times


Happy Holidays from Elliott Electric Supply! All stores will be closed on Thursday, December 25th in observance of the holiday. We will re-open on Friday, December 26th!


Elliott Electric Supply logo


We Deliver... Lower Cost, Quality Products, & Personal Service


:::


December 2025 Eaton Ad


Christmas is approaching, and you know what that means… holiday pictures!


Whether it's ugly sweaters, Santa hats, or anything in-between, you need to be ready at any moment to capture those memories. That's where Eaton and Elliott Electric Supply comes in with Eaton's full line of USB charging receptacles. On top of space for your regular plugs, these receptacles also come with USB ports right in your outlet. They come in many different configurations including with USB-A and USB-C, so you're covered no matter what cable you have. Never miss a moment again with Eaton's full line of USB charging receptacles, available at Elliott Electric Supply!


Eaton logo


:::


December Eaton Com Ad


At Elliott Electric Supply, we know that flexibility is a cornerstone of getting the job done.
That’s why we're proud to carry Eaton's Dry-Type Distribution Transformer Flex Center for our customers!


With customer driven specs and safer designs - including using air instead of oil for cooling, reducing the risk of fire - you can rest assured that these transformers are more than meets the eye. Suitable for installation indoors or in harsh environments, this industry leading product is perfect for anyone needing a reliable distribution transformer. Move out to your local Elliott Electric Supply and ask about Eaton's Dry-Type Distribution Transformer Flex Center!


Eaton Logo


:::


3M Ad


With every year getting hotter and hotter, the risk of fire gets higher and higher.
That's where 3M and Elliott Electric Supply come in!


3M's line of Fire Protection products are the perfect deterrent for fires of all kinds. For instance, the Fire Barrier Electrical Box Inserts protect electrical boxes and prevents the spread of fire in 1-2 hour rated walls. The line also includes the Fire Barrier Rated Foam FIP 1-Step, a smoke, sound and firestopping foam. There's also the Fire Barrier Sealant and the Fire Barrier Moldable Putty Pads, giving you protection on every level of your project. Head down to Elliott Electric Supply and protect yourself with 3M's Fire Protection products!


3M Logo


:::


Milwaukee Ad


Bend your conduit with Milwaukee''s M18 Fuel Branch Conduit Bender with Auto-Zero!


It comes with improved accuracy and Auto-Zero technology that automatically senses and locks in the zero-degree starting point for every bend, providing high consistency from pipe to pipe. And it's portable too, with an easy setup that allows you to work anywhere. With the reliability you've come to expect from Milwaukee, this bender will last you well into the future. And good news everyone! Milwaukee's M18 Fuel Branch Conduit Bender with Auto-Zero is available at Elliott Electric Supply. Express your way down to your local Elliott Electric Supply for more information!


Milwaukee logo


:::


ABB Res Ad


Ceiling fans are a great addition to any home. They keep us cool, they help clear the air, and they're just nice to look at.
But did you know that nearly 20,000 Americans are injured annually due to improperly installed ceiling fans?


The National Electric Code has been updated to help stop this from happening. Looking for a new, safer ceiling fan box? ABB and Elliott Electric Supply have got you covered. The new fan-rated UL listed Carlon Blue ceiling box meets the new standard and is rated for support of light fixtures up to 50 pounds and ceiling fans up to 35 pounds. That's strength to keep you and your family safe. Head down to Elliott Electric Supply to ask about ABB's Carlon Blue fan-rated ceiling boxes and keep your house cool and safe!


ABB Logo


:::


ABB Com Ad


ABB and Elliott Electric Supply are as tight as can be. Because of that, we're proud to carry
ABB's T&B Liquid-tight Systems in our stores!


It comes equipped with Power and Color Select technology, plus 3 tool free, field installable lenses, giving you the power of 27 fixtures in just one box. Light up your way to Elliott Electric Supply and check out Keystone's X-Fit Area Lights with Optic Swap today!


ABB Logo


:::


December promotional ad


Fall is finally underway with winter close behind. The leaves are falling, the wind is blowing, and
Elliott Electric Supply's 2025 Blowout Sale is on!


From November 1st to December 31st, you can visit your local participating Elliott Electric Supply to get great deals on overstocked, slow-moving, and discounted inventory! Blow through Elliott Electric Supply and fall into great savings!


EES logo


:::

Purchasing PIN security and PO authorization features


Security is at it's best when you don't have to think about it, it should just work. Elliott Electric Supply wants to
take one more worry off your plate, which is why we have ways to boost your account security!


With our PIN and PO settings, you can manage who can ship and pick up your materials. Set up a customized PIN for your will call and curbside pick-ups and enforce a specific format for your PO numbers authorizing order shipments and/or receiving. Log into elliottelectric.com to access your PIN and PO settings. Learn more here.


EES logo



Follow us on

Facebook logo Twitter logo Instagram logo

PO Box 630610 Nacogdoches, TX 75963